2021-12-03 1:48 AM
Dear Community,
In order to test the STEVAL-SPIN3204 kit, I installed the software environment as below:
I tried anything any combinaison but the problem remains: when I click to "Update" the project "6Steps_STEVAL-SPIN3204" through the "Project generation" screen as recommended, nothing happens after a long time and nothing is generated; I have to click "Cancel" to exit.
Can you give me your opinion if something can be wrong in my procedure or your instructions please? I am sure that it is just a little thing blocking...
(on the picture, the Firmware Package Version is now installed but the result is the same)
Thank you in advance.
Best Regards,
Julien
2021-12-09 11:19 AM
Did you solve the issue ? I have the same problem...
Other uses says to downgrade CubeMX (see link).
2021-12-09 11:35 AM
Just downgraded to CubeMX v6.3.0 and now it works
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.