2019-04-30 2:19 AM
I am developing a motor controller with version 5.3.3 of the MC SDK.
In the Basic tab of the Monitor, there is a Motor Power (W) indicator:
It has an upper limit of 200 Watts.
On the Registers tab, the same info can be seen:
My question is, where does this upper limit come from?
The software is configured for motor nominal DC voltage of 600.0 V and nominal current of 10.0 A, and is performing well.
The current sensor and signal conditioning setup shows a maximum readable current of 22.00A, based-on the controller I have built:
Many thanks,
Matt
2021-01-11 8:46 PM
Hi
Open your project file (*.stmcx) with text editor and search "Motor Power" in this file.
For change power gauge max value set maximum="200" to any value you want and save it.
2021-06-15 1:11 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.