2017-03-20 7:10 AM
I noticed that STEVAL-SPIN3201 is not on the supported boards list for Motor Profiler. Is there an update/path?
2017-03-22 2:28 AM
Unfortunately the Motor Profiler does not support the STM32 embedded into the STSPIN32F0 System-in-package.
In any case, you can use the Motor Profiler using one of the supported boards and then 'export' the results on the STEVAL-SPIN3201 using the MC Workbench
2021-06-27 10:04 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.