2017-01-05 4:58 AM
Hello,
I have a STM3240G-EVAL Board and the IHM023V3. My Problem is, when I connect everything, 'Overcurent' is blue in the LCD. When I press the 'Fault ack Button' all is ok, but the Motor is twitches a little bit and the 'iq ref' switch from 0 to 4000 every nearly second, so the MotorProfiler doesn´t work an show me a time out. What is wrong? Can everyone help me please?
I know, that the IHM023V3 the MP does not support, but I read, that the IHM025V1 very similar and I can take it thus.
0 Ohm resistor is remove: R51, R34, R58
soldered: R204, R66, R205
Solder Bridged soldered: SB14,15,16,10,12,11
Thanks,
Daniela
2017-05-12 2:11 AM
Hi,
Did you resolve this? I have a similar issue. See:
2021-06-27 10:05 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.