2017-05-19 12:13 AM
I try to run the motor profiler with my custom prototype SM-PSMS motor.
In this moments I hold the motor in a big vise, so the motor is impossible to move when start the current. When I run the motor profiling usually the profiling stopped for “speed feedback�? fault with a pop up with 2 recommendation:@ Most of the time this happens when the motor load change too quickly (I haven't a load, I must profiling with my custom motor reductor?)@ Sometimes it happens because the limit for Max Speed specification is too low (I try to improve the current limits but the max speed detected by the profiling is 3700RPM, the constructor of my motor specified 3000RPM.)Have you some info or advice?
The motor profiling Only 3 times is done positively. After I press 'save' and 'Play'. During 'Play' the motor run very bad.
Setup: NUCLEO-F303RE + STEVAL-IPM05F 3sh
ST Motor Profile 4.3
Motor:
Pole pair 2
Max Speed 3000 RPM
Max average Current 1A (motor profile need peak current, I write 4A)
Ld 103mH
Lq 75.25mH
so it ratio is 1.369
Vbus 320V
Thanks
Manuele
2021-06-27 10:03 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.