2022-03-01 3:21 AM
2022-03-02 6:57 AM
Hello @MRahi.3 ,
From the STEVAL-ESC001V1 schematic, there is not the required signal level adaptation layer. So this board can not be connected to the Hall sensors of your motor.
Unfortunately, there is no solution with this board. The B-G431B-ESC1 board matches this requirement.
Regards
Cedric
2022-03-02 6:57 AM
Hello @MRahi.3 ,
From the STEVAL-ESC001V1 schematic, there is not the required signal level adaptation layer. So this board can not be connected to the Hall sensors of your motor.
Unfortunately, there is no solution with this board. The B-G431B-ESC1 board matches this requirement.
Regards
Cedric
2022-03-02 7:18 AM
Thank you for your answer
2022-03-02 7:25 AM
Is the Hall effect drive mode also usable with an FOC algorithm to pilot the motor ? Or is a 6-step algorithm needed ?
2022-03-02 8:07 AM
Hall sensors present in the motor can be used with both FOC and 6-step, at the condition that the hardware support them.
Cedric
2022-03-02 8:08 AM
Ok great, thanks !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.