2022-04-04 3:42 AM
Hi,
I am using the P-NUCLEO-IHM03 STM32 motor-control pack along with a AMS AS5147U rotary sensor for speed control with Hall-effect.
The rotary sensor needs to be calibrated by setting a zero angle aligment. This is done by disconnecting the motor from the motor driver board, and connecting UVW to an external power supply. We then apply a current to the motor, resulting in locking the rotor in a fixed position and reading the angle from the rotary sensor. This angle is now treated as zero.
Does anybody know how to use the MC SDK to force a UVW pattern so that we do not rely on an external power supply to lock the rotor?
Thanks
Roar
Solved! Go to Solution.
2023-08-24 12:49 AM
For anyone else struggeling with something similar, we solved it by "Virtualizing" the angle read from the rotary sensor.
First of all, we have hijacked the function, which is used in the FOC loop
weak int16_t HALL_CalcElAngle(HALL_Handle_t *pHandle)
In normal circumstances, this function reads the RotarySensor, and populates the Handle.
When entering calibration phase, we skip the sensor readout, and instead force known electrical angles based on Hall states:
switch (Hall_State) {
case STATE_5 : {
Rotary_Sensor.VirtualElAngle = (int16_t) ((S16_60_PHASE_SHIFT / 2));
break;
} ...Next, we program a TorqueRamp based on input from user with respect to how much current we allow to flow in the stator, and run MC_StartMotor1().
As the RotarySensor feeds the FOC loop with a constant, known electrical angle, the motor is locked in a fixed position. Further calibration routine is then iterated and electrical angle is incremented to get a full rotation.
2023-08-24 12:49 AM
For anyone else struggeling with something similar, we solved it by "Virtualizing" the angle read from the rotary sensor.
First of all, we have hijacked the function, which is used in the FOC loop
weak int16_t HALL_CalcElAngle(HALL_Handle_t *pHandle)
In normal circumstances, this function reads the RotarySensor, and populates the Handle.
When entering calibration phase, we skip the sensor readout, and instead force known electrical angles based on Hall states:
switch (Hall_State) {
case STATE_5 : {
Rotary_Sensor.VirtualElAngle = (int16_t) ((S16_60_PHASE_SHIFT / 2));
break;
} ...Next, we program a TorqueRamp based on input from user with respect to how much current we allow to flow in the stator, and run MC_StartMotor1().
As the RotarySensor feeds the FOC loop with a constant, known electrical angle, the motor is locked in a fixed position. Further calibration routine is then iterated and electrical angle is incremented to get a full rotation.
2025-01-11 6:20 PM
Hi
it’s very similar to the alignment operation before start to use quadric encoder. Would you refer to that code?
hope it’s helpful.
br
RD Wang
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.