2024-03-14 7:30 PM
I would like to have a firmware example for EVLDRIVE101-HPD.
Do you know where I can find firmware examples for this board?
2024-08-23 3:16 AM
Activating the potentiometer option allows the inclusion of potentiometer.c library into the project. The pin is regularly sensed in the medium frequency task (MC_APP_PostMediumFrequencyHook_M1) and any change applied as a speed ramp.
The UART is used by the MotorPilot to communicate with the microcontroller. You can launch the GUI from the corresponding icon on top of the workbench window.
I suggest to introduce the MC_StartMotor1() call once you are sure the motor is properly controlled by the MotorPilot. If the motor spins for only 1-2 seconds, it is likely a problem with speed PID gains leading to overcurrent or wrong connection or improper connection position of the sensors.
Alessio
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.