2025-12-09 5:15 AM
Hi All,
I am currently planning a custom motor control design based on the STM32G431CUB6 microcontroller for a 3-phase inverter application.
Before finalizing my PCB design, I would like to clearly understand the firmware flashing and runtime communication possibilities, especially related to Motor Pilot and real-time monitoring.
I kindly request your clarification on the following points:
Your guidance will help me finalize my hardware design and production programming strategy correctly.
2025-12-09 6:18 AM
@Sujibarathi123 wrote:Hi All,
I am currently planning a custom motor control design based on the STM32G431CUB6 microcontroller for a 3-phase inverter application.Before finalizing my PCB design, I would like to clearly understand the firmware flashing and runtime communication possibilities, especially related to Motor Pilot and real-time monitoring.
I kindly request your clarification on the following points:
- Is the use of ST-LINK mandatory for flashing the firmware into the STM32G431CUB6 during development?
- Does Motor Pilot software communicate with the MCU only through ST-LINK, or can it also operate via UART?
- For real-time monitoring of parameters such as RPM, DC bus voltage, current, and motor status using Motor Pilot, is ST-LINK compulsory?
Your guidance will help me finalize my hardware design and production programming strategy correctly.
1. Yes ST-Link is required for flashing the software. I am not sure what is the exact question.
2. Motor pilot communicates using UART not ST-Link, ST-Link only for flashing.
3. No ST Link not required, UART is required.
2025-12-09 8:04 PM
Hello STuser2,
I am using the B-G431B-ESC1 as a reference design.
On the original ESC board, the STM32F103CBT6 (on-board ST-LINK/V2-1) provides:
SWDIO/SWCLK for programming & debugging the STM32G431
Virtual COM port (UART TX/RX) used by Motor Pilot for real-time communication (speed, voltage, current, position)
I am not using the on-board STM32F103CBT6.
I plan to remove this STM32F103CBT6. and instead use an external STLINK-V3SET / STLINK-V3MINI.
My question:
Can I connect the STM32G431 UART pins directly to the STLINK-V3SET/V3MINI “Virtual COM Port” pins and use Motor Pilot normally?
In short:
If I wire
G431 TX → STLINK-V3 UART RX
G431 RX → STLINK-V3 UART TX
GND → GND
Will Motor Pilot successfully connect and control the motor over MCP protocol (start/stop, speed monitoring, etc.)?
I want to confirm that the STLINK-V3 UART interface works the same as the on-board VCP used in B-G431B-ESC1.
2025-12-09 8:57 PM
Yes it is possible i think.
The user manual refers to them
Electronic speed controller Discovery kit for drones with STM32G431CB - User manual
And the STLINK V3 debugger has this information
So it should be possible.
2025-12-09 10:33 PM
Thanks for the immediate response.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.