STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

motor is drawing more current than expected

Hello all,I’m using NUCLEO F302R8 and IHM08M1 for motor control. While the motor runs, it gradually heats up to around 85°C and draws more current than its rated value in no-load conditions.while using the IHM07M1, the motor's heating seems normal, b...

hashiR by Associate III
  • 6441 Views
  • 13 replies
  • 2 kudos

Resolved! How to control a Maxon BLDC with hall sensors

Hi,I'm trying to drive a Maxon 574741 BLDC motor with hall sensors, using your STEVAL-SPIN3204 evaluation board. I have installed MC Workbench, STM32CubeMX and the STM32CubeIDE. I'm rather new to motor control and the parameter setup for my motor in ...

LeiSve by Associate II
  • 3105 Views
  • 2 replies
  • 0 kudos

I will create code for discovery kit 'B-G431-ESC' as described in UM2516 chapter 6.1 step 2 and 3 but I get error when compiling with STM32CubeIDE . Is there a more detailed description for generation or an example for this evakit?

I use MCSDK v5.4.7 and STM32CubeIDE 1.6.1. Project generation with MCSDK is successful but when I try to build code with the IDE it ends with fatal error "sto_cordic_speed_pos_fdbk.h: No such file or directory". Run code generation with an other exam...

JMust.1 by Associate
  • 1774 Views
  • 2 replies
  • 0 kudos

AS5600 I2C Communication

Hi.I am trying to communicate with AS5600 Position Sensor. We are using I2C communication for this purpose. Using STM32F439ZIT6 chip , running chip at 168 MHZ clock. We are sommunicating with the sensor at Fast mode 400000 speed. Connection seems OK ...

V.D.T: by Associate
  • 3331 Views
  • 1 replies
  • 1 kudos

STM32 NUCLEO BOARD AND BOOSTXL-DRV8323RS

Hi,I am trying to run a 3-phase BLDC motor using the DRV8323 driver in 1xPWM mode with a Hall effect sensor. I am also using the Nucleo WB55RG board to generate a 20kHz PWM signal.The motor is spinning, but there is audible noise, which decreases onl...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.