2021-10-22 2:49 AM
I use MCSDK v5.4.7 and STM32CubeIDE 1.6.1. Project generation with MCSDK is successful but when I try to build code with the IDE it ends with fatal error "sto_cordic_speed_pos_fdbk.h: No such file or directory". Run code generation with an other example project works well. So I asume that my tool chain is okay.
2021-10-22 8:01 AM
Hello @JMust.1 and welcome to the Community :)
I think you don't have the Include Paths set up coherently.
You have to review the defines and the include file paths for your project: Go to Project options ->C/C++ tab->Include paths and add new paths to your include directories.
Feel free to share your update and solution, It should be helpful for the Community =)
When your question is answered, please close this topic by choosing Select as Best.
Imen
2025-01-17 11:09 PM
hi,
I have been trying to run PMSM motors with B-G431B-ESC1, I follow the steps given in the user manual,
1. I profile the motor and save the parameters
2. use the motor control workbench to generate a project, and generate source code,
3. run it in Cube IDE to flash it on the development board.
However, I am unable to run my motor with that source code. The motor doesn't even start. I also face inconsistency when running the motor with the same source code on different occasions. What could be the issue, and what should I do to resolve this issue?
since the profiler is working, where can I get a profiler code based on which the profiling .hex file is created to debug the issue?
Thank you,
Madhav
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.