STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! what is the voltage range for X-NUCLEO-IHM03A1?

According to product page X-NUCLEO-IHM03A, this motor driver voltage range should be between 10.5 V to 85 V. But I got a sample I do see Vin max printed as '50V'. Can someone from the nucleo explain which max voltage spec I should choose?

轩郭.1 by Associate
  • 1292 Views
  • 1 replies
  • 0 kudos

Resolved! hi everyone ! need some help with STM32F401RE i m gana read 6 analog input using ADC with DMA and timer then i wana call the values from the memory to use it in the same time i wana made PWM output for my servo motor .

 I solved ADC and DMA part but i have problem whit calling the the values from memory and with PWM output that my servo motor cant work any way . plz help me:smiling_face_with_smiling_eyes: .NOT: im new in stm32

Halra.1 by Associate II
  • 5456 Views
  • 12 replies
  • 0 kudos
TB by Associate III
  • 2270 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F FOC SDK User Manual

Is there a newer version for the DocID18458? UM1052 is a very nice (but outdated) user manual for the FOC SDK for STM32F microcontrollers, it is more complete than UM2374 but has not been updated, or at least I can not find a newer version, since Sep...

kswarm by Associate II
  • 2835 Views
  • 1 replies
  • 0 kudos

Anyone else having problems with Nucleo F302R8 with the IHM08M1 driver board to run a motor using the X-Cube SPN8 6-step algorithm?

We are currently using a Nucleo F302R8 with the IHM08M1 driver board and the Bull Running BR2804 motor provided with the development kit. We are using ST's X-Cube SPN8, 6-step software and compiled it, unmodified, with Keil MDK 5. Unfortunately, the ...

MBlan.1 by Associate
  • 1267 Views
  • 3 replies
  • 0 kudos

Resolved! Where can I download MC SDK V4.3?

I am having the P-Nucleo IHM001. I am trying to generate code using ST Motor Control Workbench, but after building and dumping the code in the controller, the motor is not spinning and two faults are showing up:FOC faultSoftware errorI want to try ol...

PPati.1 by Associate II
  • 3668 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.