STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

Resolved! IAR embedded WB from CubeMX to drive IHM003 motor control dev kit error : Error[Li016]: size limit exceeded. The application needs 0x86b6 (34'486) bytes

When I run code in IAR embedded WB from CubeMX to drive IHM003 motor control dev kit initial project (same as in getting started video) , I have got this error Error[Li016]: size limit exceeded. The application needs 0x86b6 (34'486) bytes, which is g...

AGuze.1 by Associate
  • 2136 Views
  • 3 replies
  • 0 kudos

Resolved! Corrrect way to update frequency (ARR) to generate step pulse for stepper motor using stepper driver drv8711 and stm32 micro controller.

Hello,I am Sai hope you are doing well I am facing some issues with the timers .I am using stm32f4,f7 micro controller to pulse step input of stepper motor driver. I have configured my timer using HAL layer. i want sweep the frequency from 100hz to s...

steja by Associate II
  • 2608 Views
  • 3 replies
  • 0 kudos

Resolved! Is a safe way to convert others ADC channels using the same interrupt mechanism employed by a FOC 4.0 library?

Hi,I'm here to ask if someone knows a safe way to convert other analog sources using the ADC macrocellsof a STM32F407ZE MCU used to spin a BLDC motor by means of a FOC 4.0 library.I mean, is there a way to correctly hook my code to the ADC IRQ Handle...

I'm looking for motor driver board

Hi! I'm a beginner and need help ~i have a board with Nucleo-F411RE.so I'm just looking for using motor driver board with this one could u plz recommend any one ?Thx in advance~~ ​

Brushless motor control using a STM32F302RB

Hi!I'm trying to control a brushless motor using a STM32F302RB and X-NUCLEO-IHM08M1.But the motor is not spining!!I need your help !best regards!I'm using mbed online compiler to configurate TIM1_CH1 pin (PA8)�? TIM1_CH1N pin (PA7)�? TIM1_CH2 pin (PA...

OS'HI by Associate II
  • 5428 Views
  • 8 replies
  • 1 kudos

Resolved! STEVAL-ISC004V1 Configure PDO does not work

i bought your STEVAL-ISC004V1 together with NUCLEO-F072RB to configure to configure NVM over I2C. For this you have the tool: STSW-STUSB001Now i really tried to connect everything like the minimal description in the UM2254 of the STSW-STUSB001, but ...

REtti by Associate
  • 2189 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.