STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Resolved! How to connect STM3210B-EVAL to MC Workbrench v.2.1.0?

Hello! I am s student of NSTU. Our faculty (of Mechatronics and Automation) bought a STM3210B-MCKIT two years ago. My supervisor made me to give a life to this kit two weeks ago. So i have next problem:I have read all kit's documentation. And I have ...

GSido.3 by Associate
  • 1458 Views
  • 1 replies
  • 0 kudos

Resolved! EVAL-KIT-ROBOT-1

Hi,have a question, i don't understand the difference in holding register from low register (address 0) and high register(address 1). I used QmodBus 0.2.1 and if i set degree in low register i have no problem.. But in a High register if set a value >...

DBrag.1 by Associate II
  • 4561 Views
  • 9 replies
  • 1 kudos

Measure time between encoder counts wtih STM2f439ZI

Hello, I'm super new to all this STM32 stuff so bear with me please.I'm using a Nucle board with an STM32f439ZI and I want to measure the speed of my motor. So far I managed to count the increments of my incremental encoder. I did that by configurati...

Resolved! Why all the routines, to handle the DAC output, in the STM32Fxxx_nucleo_ihm08m1 are without code (completely empty)? i.e void START_DAC() { }, void STOP_DAC() { }, void SET_DAC_value(uint16_t dac_value) { }

The 6.2 paragraph of document DocID029868 (Rev. 2), page 34, appears to be reporting incorrect information.Furthermore, pin PA4 seems to be connected to the speed reference (potentiometer) not to one of the DAC outputs as reported in the mentioned d...

RStef.2 by Associate
  • 1729 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.