2021-03-09 11:41 AM
The 6.2 paragraph of document DocID029868 (Rev. 2), page 34, appears to be reporting incorrect information.
Furthermore, pin PA4 seems to be connected to the speed reference (potentiometer) not to one of the DAC outputs as reported in the mentioned document.
I'm using ihm08m1 board with nucleo-F401re.
Solved! Go to Solution.
2021-03-11 6:25 AM
Hi @RStef.2 ,
The DAC peripheral is not available in the STM32F401RE, this is the reason why the DAC routines are empty.
These functions are not empty in the example with the NUCLEO-F302R8 instead.
To emulate the DAC functionality you can use a timer generating a square wave and change its duty cycle.
Low-pass filtering this signal provides an analog voltage between 0V and 3.3V proportional to the duty cycle.
By default the PA4 is connected to the potentiometer. If you want to use PA4 as a DAC purposes
you can disconnect R181 and connect R76 so you can have the line mapped on the connector J7 and on the current REF net.
Have a nice day !
2021-03-11 6:25 AM
Hi @RStef.2 ,
The DAC peripheral is not available in the STM32F401RE, this is the reason why the DAC routines are empty.
These functions are not empty in the example with the NUCLEO-F302R8 instead.
To emulate the DAC functionality you can use a timer generating a square wave and change its duty cycle.
Low-pass filtering this signal provides an analog voltage between 0V and 3.3V proportional to the duty cycle.
By default the PA4 is connected to the potentiometer. If you want to use PA4 as a DAC purposes
you can disconnect R181 and connect R76 so you can have the line mapped on the connector J7 and on the current REF net.
Have a nice day !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.