2021-03-23 3:04 AM
2021-03-23 6:03 AM
Welcome, @SKhar.1 to the community!
If you really want to use it, you should be able to find the System Workbench for STM32 here.
But for some years now, ST has been recommending using STM32CubeIDE instead, which can also be used to import AC6 projects.
Regards
/Peter
2021-03-23 6:53 AM
Hello Peter.
Thanks for answer.
I need help.
I watch video tutoreals about this programs and made everithing like in video,but program didn't working.
When I'm triyng working with AC6 after generation and goes Eclipse IDE,when I click green arrow after choosing project,it goes error.
I will send photo and video and if you can,help me please.
If you can,I will contact You on facebook or Viber.
Sincerely Sulkhan
2021-03-23 9:22 AM
System Workbench for STM32 is community supported and you can usually get support in the forum, maybe a nice community user has an answer here as well.
However, ST cannot otherwise support System Workbench for STM32.
Good luck!
/Peter
2021-05-27 10:41 PM
The question has been moved to the "STM32 Motor Control" section (the question is about the STM32 SDK).
Best regards
Laurent Ca...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.