2021-04-15 3:23 AM
Hello, I have a question regarding the use of the timer function xor input for the hall sensor in the BLDC motor, how do I read the first rotor position to start, then I understand that each timer interrupt changes the commutation.
2021-05-27 10:34 PM
The question has moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 SDK).
Best regards
Laurent Ca...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.