STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1836 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4990 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9743 Views
  • 5 replies
  • 3 kudos

Resolved! STSPIN948 evaluation board: motor not rotating

Hello,We are currently performing tests on stepper motor driver boards.We are using a NUCLEO-F401RE board, which works correctly with the X-NUCLEO-IHM14A1: the motor rotates normally using the interface provided by STSPIN Studio 2.0.However, while ke...

Logan10 by Associate
  • 355 Views
  • 3 replies
  • 0 kudos

Resolved! CSConnect Errors When Generating Custom Project

Hello,I am working on a custom FOC Inverter Board.  I am trying to assign the pins for current sensing, but I keep getting warnings.  I am using an STM32G431CBT6 MCU, and I completed all the other pin assignments without issue.  Here is the Current S...

reesed13_0-1779544074338.png
reesed13 by Associate II
  • 336 Views
  • 6 replies
  • 2 kudos

STM32MotorControl project with RTOS (RTX5)

Are there any examples on how to integrate the project exported from ST MC Workbench, which runs in systick for medium priority tasks and in DMA callback for FOC algorithm, into a custom RTX5 (or any other RTOS - CMSIS RTOS) project?I have tried movi...

priorities.png
Klemen63 by Associate
  • 130 Views
  • 1 replies
  • 0 kudos

Resolved! STEVAL ESC001V1 Motor Pilot Graph

I am trying to plot reference speed and measured speed on graph in Motor Pilot. But in graph why measured speed is coming before reference speed? I tried it at different speeds but response coming is same.

ref_meas.png

Motor control with resolver

Good afternoon,I am working with the STSW-TTM005 example for a resolver-equipped motor and encountered an issue:Link: STSW-TTM005 | Product - STMicroelectronicsThe motor does not rotate, but instead oscillates between windings.In sensorless mode, the...

P-NUCLEO-IHM03 giving driver protection fault

Good evening, I am trying to use a P-NUCLEO-IHM03 pack.I have generated the project using the X-CUBE-MCSDK version 6.4.2 and STM32cubeMX version 6.17.0, built and flashed the project on the board. The problem is that as soon as I try to start the mot...

giulioTam_0-1779283331625.png giulioTam_1-1779283649343.png Screenshot 2026-05-20 152342.png giulioTam_2-1779283920065.jpeg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.