STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Problem opening project with TrueStudio

Hello,I'm trying to run my motor with a nucleo F303RE and IPM08B but I can't reach a succesful compiling. I tried with X-CUBE-MCSDK 5.1.1 and 5.3.3 and cube 5.0.1 and 5.1.0 without a succesful result. When I try to compile the atollic gives me a lot ...

A?�lv by Associate
  • 2760 Views
  • 5 replies
  • 1 kudos

MCSDK for PMSM at low speed problem.

Hello everyone.I'm using MCSDK tool to generate code for FOC PMSM. Motor work well when I set a high rpm, above 1000 rpm, but when I set a low rpm, like 100, 200, ... motor just spin a very little angle and stop. I guess the problem caused by PI spee...

Any BLDC position control library in MCSDK?

Hi STM team,I am applying your software and hardware toolkit to realize BLDC position control. I plan to use STEVAL-SPIN3201 together with quadrature encoders as the hardware solution, but I find that there is no position control function in the MCS...

JCHEN.4 by Associate II
  • 1667 Views
  • 3 replies
  • 0 kudos

How I use the gap drive

I get the kit STEVAL-HKI001V1 without software, I tryed to use the MotorControl Workbech to generate a code project , and I checked the "use STGAP1S gap drive" like the photo, I builded the project , but failed ,and it prompted that "../MCSDK_v5.2...

mcen by Associate II
  • 1182 Views
  • 1 replies
  • 0 kudos

Always have hard faults on MCSDK 5.4.0

Hi all,As title, I used MCSDK 5.4.0 and it always generated a hard fault when starting motor.This issue cannot be found in previous versions.It can only happen on sensorless FOC but hall sensors.Can any one checked the prebuilt MCSDK 5.4.0?One more q...

JHsu.13 by Associate
  • 1962 Views
  • 2 replies
  • 1 kudos

Payload length in Serial Communication in MCSDK

Hi everybody,I read the document UM1052 and in this document we can see this "Payload_Length: the total number of bytes that compose the frame payload". My question is: does the payload length include Payload_length byte itself and CRC ?Precisely wha...

Randy1 by Associate III
  • 1305 Views
  • 2 replies
  • 0 kudos

SVPWM implementation with MCSDK

Hi,I have studied UM1052 user manual about vector control implementation on PMSM. But I have two major problems. The first one is with the SVPWM implementation on sector 4.11 and the other one is "Circle limitation" on sector 4.12.1 .I am actually lo...

Resolved! EVSPIN32F0601S3 + ST Motor Profiler

Hey. When will it be possible to add the EVSPIN32F0601S3 board to the ST Motor Profiler? Or which one to choose from the proposed for determining the parameters of the electric motor?

SLodo.1 by Associate
  • 2187 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.