STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

STM32G4 ADC1/2 Dual Mode Reading

Hello community,I am using STM32G474 for my FOC application and I am a bit confused about the ADC modes.Since the G4 series has a wide range of ADC modes, which ADC mode is best for 2 or 3 phase current sensing in FOC applications?Is the "dual inject...

batuhanky by Associate III
  • 513 Views
  • 1 replies
  • 0 kudos

X-NUCLEO-IHM08M1 with NUCLEO-U575ZI-Q

Does anyone know how to connect X-NUCLEO-IHM08M1 with NUCLEO-U575ZI-Q?CN11 and CN12 of NUCLEO-U575ZI-Q will be connected to CN7 and CN10 of X-NUCLEO-IHM08M1 respectively?  Pin 1 of CN11 and CN12 are connected to Pin 1 of CN7 and CN10?Thank you

Suthan by Associate II
  • 363 Views
  • 1 replies
  • 1 kudos

EVLSERVO1 multi motors

 Anyone tried to control more than one motor with the EVLSERVO1?The scenery that I mean is like: the ELVSERVO1 is 3kW, so I would control 4 motors of 500W each and give to the EVLSERVO1 the reference (hall sensors) of one of the 4 motors.Did anyone t...

ST Motor Pilot

 Able to generate a code (446+IHM08M1) and spin the BLDC motor. Configured a serial port in my generated code with 19200 Baud Rate.Want to monitor all the parameters using ST Motor Pilot.How to make use of the ST Motor Pilot?Does it Auto detect the H...

ASPEP - how is synchronisation done ?

Hello thereI´ve consulted documents explaining the ASPEP - I´m still wondering how synchronisation is done. -Like is there a unique token / value / ASCII character marking the start or end of a telegram?E.g. the NMEA protocol for GPS antennas use the...

Humming Noise at High RPM Using Sensorless FOC

Hi Everyone,We are using an STM32F401RE Nucleo board with the IHM16M1 power board, running a sensorless FOC algorithm generated using ST Motor Control Workbench. The motor parameters were averaged over several runs using ST Motor Profiler, and the co...

speed.PNG
Mani2 by Associate III
  • 2080 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.