STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4993 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9747 Views
  • 5 replies
  • 3 kudos

STSPIN32G4 Power Consumption Reduction

I customized a version of the EVSPIN32G4 eval board to spin my 2 pole pair BLDC 24V 2A motor in sensorless FOC mode. My schematic is similar to the eval schematic. When the motor is spinning the STSPIN32G4 on my board is getting to 65 degrees C which...

WSega.1 by Associate II
  • 1482 Views
  • 2 replies
  • 0 kudos

STEVAL-PTOOL1V1 sample code

helloI have been purchased one of STEVAL-PTOOL1V1 evaluation board.I am going to develop sample code which provided by company, but some errors occurred in building new file process by IAR & Keil IDE.errors of following:no definition for "MC_Core_St...

amoos.11 by Associate II
  • 4647 Views
  • 10 replies
  • 0 kudos

Installing Motor Profiler 5.4.3

My computer crashed & I needed to reinstall all my tools on another system. Both are Windows 10 64x. I can't get the Motor Profiler 5.4.3 to connect on the new system. When I try to connect I get a message it can't find the MFC100.dll. I installed th...

BTrem.1 by Senior II
  • 1966 Views
  • 3 replies
  • 1 kudos

STM32G4 Window Comparator Alternatives

I am designing a motor controller PCB that uses an STM32G4 MCU (since the CORDIC accelerator and FPU will be useful in my application). One of the required features for this project is cycle-by-cycle current limiting for a BLDC motor. I have two phas...

BPaik by Senior
  • 2307 Views
  • 3 replies
  • 0 kudos

I am able to generate a complementary PWM signal. However due to hardware changes I would need to add a dead time. Regardless the value I am setting in the BDTR register there is no dead time at the output.

// InitialisationTIM1->PSC = (FOSC/(PWM_FREQ * PWM_STEPS)) - 1;    // Timer clock TIM1->ARR = PWM_STEPS - 1;                        // Auto reload TIM1->BDTR = 0;                                    // SafetyTIM1->CCER = 0;TIM1->CR2 = 0;TIM1->CCMR1 = ...

Inline current sensing problem for ST mcsdk ?

I try to drive (FOC) BLDC motor with STM32G474RE MCU. I use a custom board. I use INA240A1 for inline current sense. Can I use 3 shunt inline current sense method for ST mcsdk ? In STs evaluation boards typically low side shunt resistors are used for...

0690X00000BuyaKQAR.png
HK by Associate II
  • 2195 Views
  • 4 replies
  • 0 kudos

Resolved! ACIM motor

Have Nucleo-64 STM32L476RG and STEVAL-IPM15B , i plan to test VFD and FOC drive for pump with ACIM motors , but the workbench motor control is for pemanent magnetic motor !!are there any additional library or sdk to handle ACIM motor ?

BAbde.1 by Associate
  • 2080 Views
  • 3 replies
  • 0 kudos

ST MC Workbench code generation error

I bought STEVAL-SPIN3201 for development. I installed ST MC-WB , CubeMX and CubeIDE to on my PC. When I tried to generate code by MC-WB it is says "STM32CubeMX not found". But as I said it is already intalled. What could be the reason?

Dkoşa.1 by Associate
  • 1765 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.