2020-04-23 5:03 AM
Have Nucleo-64 STM32L476RG and STEVAL-IPM15B , i plan to test VFD and FOC drive for pump with ACIM motors , but the workbench motor control is for pemanent magnetic motor !!
are there any additional library or sdk to handle ACIM motor ?
Solved! Go to Solution.
2021-06-28 5:37 AM
Dear @BAbde.1
There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.
Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .
Best regards
2021-06-14 11:36 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
2021-06-28 5:37 AM
Dear @BAbde.1
There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.
Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .
Best regards
2021-07-21 2:28 AM
thanks alot , where i can dowload it please ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.