STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Controlling Brushless motors with an ESC

I'm working on using an STM32F446RE board to control two brushless motors using a SimonK ESC (https://www.amazon.com/dp/B07NMJRJKJ?psc=1&ref=ppx_yo2_dt_b_product_details) (sorry I don't know how to shorten the link) now normally these types of produ...

TSwin.1 by Associate
  • 1198 Views
  • 0 replies
  • 1 kudos

Hello everone, I am new to STM and I have a STEVAL-spin3201. I want to drive a BLDC motor named U65HN-024KS. When using motor pilot program, it starts spinning and over current fault just appears and stops.

I am not sure that I am using the proper motor. Because, according to the setting in motor section, it should be PMSM and be controlled with FOC algorithm. Since I only know that this motor is BLDC, I dont know that if my motor is supported by this a...

MSaff.2 by Associate II
  • 1696 Views
  • 3 replies
  • 0 kudos

(Bug Report) When using encoder, the generated code has a few defects - speed calculation is not reliable, no speed reliability check, and no scheme to clear speed feedback fault

(Environment)MC_SDK 5.Y.3 + STM32CubeMX 6.3.0 with HAL + IAR EWARM 8.5(Hardware)custom board based on F446RE + custom power board + Low Voltage BLDC motor with Encoder(Control Mode)Speed Control​(What I found)(1) speed calculation is not reliable[ EN...

THA.1 by Associate II
  • 2559 Views
  • 4 replies
  • 0 kudos

Bug report :Max speed with Hall sensors

Dear MCSDK team,We met a difficulty using Hall sensors as our primary speed and position sensor.When setting a mechanical speed higher than UINT16_MAX / nb_pair_poles / 2 the value of hMaxReliableElSpeedUnit is overflowing in the Hall_Init function. ...

ANICO.1 by Associate III
  • 1615 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.