STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

CAN messages read from car using STM32F407VE

I have motor controller and i have to communicate with it using can bus, problem is the manufacturer hasn't provided can can codes . I want to display all the messages available on bus so i can manually figure out the codes for specific functioncan a...

DGajb.1 by Associate
  • 1194 Views
  • 0 replies
  • 0 kudos

Resolved! Why ST does not provide a support?

Look at this forum! Almost no one is getting answers for their questions from ST!I have received one answer from ST only. I guess I am lucky. Thank you. I asked 3 more questions - no luck.I have opened the case with online support, It was "escalated"...

EShaw.1 by Associate II
  • 2503 Views
  • 6 replies
  • 0 kudos

Resolved! Details of SPD_GetAvrgMecSpeedUnit

I asked a question before on the routine SPD_GetAvrgMecSpeedUnit but the answers did not address what I was looking for. https://community.st.com/s/question/0D53W00000xsTlzSAE/information-on-the-c-code-procedure-spdgetavrgmecspeedunit-This routine re...

0693W00000JMmwhQAD.png
BTrem.1 by Senior II
  • 2756 Views
  • 3 replies
  • 0 kudos

USART3 stops working after code update.

I have a motor control board built around the STM32F446RET6. I was updating code using motor control workbench to alter the control parameters.After an update, I was no longer able to use the motor control workbench console to communicate with the bo...

DTard.1 by Associate II
  • 6363 Views
  • 12 replies
  • 0 kudos

Resolved! STEVAL-SPIN3202 Correct positions of the jumpers

Dear ST,Could you please advice on the correct positions of STEVAL-SPIN3202 jumpers to run an example with ST MotorPilot.J9 - BOOT0 Open or closed? J7 - RX - TX Open or closed, Could you please explain why would we need to connect RX and TX? Which o...

0693W00000Ka6sLQAR.png 0693W00000Ka6yJQAR.png 0693W00000Ka6zbQAB.png
EShaw.1 by Associate II
  • 1821 Views
  • 2 replies
  • 0 kudos

Deadtime

First thingI am trying to XOR, 3 pwm's and If the xor output is 1 "motor is on" otherwise "motor is off".I am getting 90ns deadtime. I mean between the pwm's there is some gap. How to encounter this situation? ( I wnt to use a gpio and Im using a nuc...

Vmere.1 by Senior
  • 1152 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.