2022-01-19 12:48 AM
(Environment)
MC_SDK 5.Y.3 + STM32CubeMX 6.3.0 with HAL + IAR EWARM 8.5
(Hardware)
custom board based on F446RE + custom power board + Low Voltage BLDC motor with Encoder
(Control Mode)
Speed Control
(What I found)
(1) speed calculation is not reliable
[ ENC_CalcAvrgMecSpeedUnit() in encoder_speed_pos_fdbk.c ]
Encoder direction and UP(overflow/underflow) count are used to calculate the delta.
This algorithm lead, however, to an incorrect result in the following case:
This case can happen when the motor is hunting around zero speed, including encoder alignment.
=============================================================
if ( directionSample == LL_TIM_COUNTERDIRECTION_DOWN ) {
/* encoder timer down-counting*/
OverflowCntSample = ( CntCapture > pHandle->PreviousCapture ) ? 1 : 0;
pHandle->DeltaCapturesBuffer[pHandle->DeltaCapturesIndex] =
( int32_t )( CntCapture ) - ( int32_t )( pHandle->PreviousCapture ) -
( ( int32_t )( OverflowCntSample ) + OFbit ) * ( int32_t )( pHandle->PulseNumber );
}
=============================================================
(2) no speed reliability check
[ TSK_MediumFrequencyTaskM1() in mc_task.c ]
=============================================================
__weak void TSK_MediumFrequencyTaskM1(void)
{
...
(void) ENC_CalcAvrgMecSpeedUnit( &ENCODER_M1, &wAux );
...
case RUN:
MCI_ExecBufferedCommands( &Mci[M1] );
FOC_CalcCurrRef( M1 );
break;
....
}
=============================================================
=============================================================
__weak void TSK_MediumFrequencyTaskM1(void)
{
...
bool IsSpeedReliable = HALL_CalcAvrgMecSpeedUnit( &HALL_M1, &wAux );
...
case RUN:
MCI_ExecBufferedCommands( &Mci[M1] );
FOC_CalcCurrRef( M1 );
if( !IsSpeedReliable )
{
STM_FaultProcessing( &STM[M1], MC_SPEED_FDBK, 0 );
}
break;
....
}
=============================================================
(3) no scheme to clear speed feedback fault once happened
[ SPD_IsMecSpeedReliable() in speed_pos_fdbk.c ]
"ENCODER_M1._Super.bSpeedErrorNumber" is incremented to its max(default:3) then generating an alarm, but no state transition or API to reset this value to zero.
2022-01-25 4:39 PM
I added additional issues after more test.
2022-02-14 3:51 PM
Please could someone ST member clarify this issue?
2022-03-02 10:17 AM
Hello @THA.1 ,
Thanks for your post.
I do agree with you. We have an issue if we have a speed inversion between two sampling events. This could happen if the motor speed is around 0.
We need to internally check what would be the best way to solve this tricky case.
Regards
Cedric
2022-03-02 4:15 PM
Thank you for your reply.
Just a traditional way would be a good choice if sampling frequency is high enough - determining overflow/underflow by the amount of change of the counter.
Regards,
THA.1
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.