STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

ADC injected mode can't interrupt?

I try to transplant the Three-Shunt FOC project based on STM32G431RB supported by MCSDK to STM32G431C8.But The ADC interrupt is never called.I comment the code below in function R3_2_ADCxInit,the interrupt works.LL_ADC_INJ_SetQueueMode( ADCx, LL_ADC_...

Lzhiy.1 by Associate II
  • 1561 Views
  • 0 replies
  • 0 kudos

Getting started with MCSDK and P-NUCLEO-IHM002

I'm using SDK version 5.Y.4.I start by using the motor profiler and the included motor, with the settings 7 pole pairs, 18000 max rpm, 2.8Apk, 12V. It makes a profile, but gives warnings that stator resistance and stator inductance are < 1.I can use ...

Resolved! There is such a document: "AN5464-Position control of a three-phase permanent magnet motor using X‑CUBE‑MCSDK or X‑CUBE‑MCSDK-FULL"

Hi!There is such a document: "AN5464-Position control of a three-phase permanent magnet motor using X‑CUBE‑MCSDK or X‑CUBE‑MCSDK-FULL"It describes the method of setting the PID controller. It is necessary to reset all coefficients and gradually incre...

Encoder Alignment With Phase Swapping

Hello, I am working on trying to get a BLDC motor spinning and I have stumbled across some behaviour I don't fully understand. First, some details about the hardware and software I'm using:SoftwareST MCSDK v5.4.7HardwareBoard:Custom board with STM32L...

JMari.7 by Associate
  • 1279 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.