STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4993 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9747 Views
  • 5 replies
  • 3 kudos

MCSDK 5.y.x 6-step firmware generation

Hello,I have STEVAL-SPIN3204 board and a BLDC motor with hall sensor.So, I try to generate a firmware with 6-step control and hall sensors.ST Motor Control workbench (v5.y.4) generate the firmware.But, the source code folder have not MCLib6Step folde...

AShin.5 by Associate II
  • 1578 Views
  • 3 replies
  • 0 kudos

Sensorless FOC - sudden motor rotation change

Hi CommunityI'm using the following setup:MC Motor Control Workbench v6.0.0STM32 FW V1.5.0 (HAL)Power + Control Board: B-G431B-ESC1Observer + PLL (Sensorless)Motor 10 pole pairMech. Speed 200rpmThe motor starts and ramps up to 200rpm.It can now happe...

RReic.2 by Associate II
  • 4420 Views
  • 5 replies
  • 0 kudos

Resolved! Customer is using STM32L4 and L6235Q

The customer was looking for a lock function from its BLDC motor driver. They were advised to use the “dynamic braking�? function of their motor driver, it seems - from what I understand. The Dynamic braking function does not offer a true locking fun...

EHD by Associate II
  • 1379 Views
  • 1 replies
  • 0 kudos

FOC Motor Direction Control

I've implemented an FOC motor control algorithm from scratch (e.g. not using any libraries) and it works well. I'm generating sine waves to drive the MOSFETs via a lookup table.All this works and the motor turns in an anti-clockwise direction. How do...

jerry2 by Senior
  • 1761 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.