2022-05-12 12:20 PM
The customer was looking for a lock function from its BLDC motor driver. They were advised to use the “dynamic braking�? function of their motor driver, it seems - from what I understand. The Dynamic braking function does not offer a true locking functionality, unfortunately. Dynamic braking will allow the motor to drift from a stopped position, if the load can overcome the mechanical frictions and backdrive the motor and its transmission. Think of it as adding a lot of viscosity into a mechanism; that’s what the Dynamic Braking functionality of a BLDC motor driver chip provides. In the customer’s situation, closing the loop on position (simple Proportional closed-loop is probably sufficient in this case) would keep motor in its stopped position, even if the load tries to backdrive the motor.
Application: Tourniquet. After reaching proper pressure, the tourniquet must stay in position not to allow the release of pressure. Dynamic Braking will allow a slow release of the pressure, which is unwanted, in this case. A closed loop system in the MCU would prevent pressure release when in stopped position.
Solved! Go to Solution.
2022-05-13 2:02 AM
Hello @EHD,
the L6235 Brake function can be used to quickly stop the motor while it is running (making a short-circuit across the motor windings).
If you want to keep a position it is necessary to apply a torque.
If I understood well the application if you limit the torque is like holding the tourniquet in tension with a maximum constant force.
2022-05-13 2:02 AM
Hello @EHD,
the L6235 Brake function can be used to quickly stop the motor while it is running (making a short-circuit across the motor windings).
If you want to keep a position it is necessary to apply a torque.
If I understood well the application if you limit the torque is like holding the tourniquet in tension with a maximum constant force.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.