STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

STEVAL-SPIN3201 not detecting STLink

I have purchased the STEVAL-SPIN3201 board, but the STM32Programmer does not detect the ST-Link, the LEDs are not getting ON. I also purchased the external ST-LINK V2, with that i tried connecting and erased the memory. The USB driver also having pro...

0693W00000NrDGeQAN.jpg 0693W00000NrDGZQA3.jpg
JDesi.1 by Associate II
  • 5152 Views
  • 11 replies
  • 0 kudos

Running speed control with FOC using the X-NUCLEO IHM08M, what causes the 0.1 Hz "step-wave" on top of the DC bus ?

If I measure the DC supply voltage for my X-NUCLEO-IHM08M driver board - connected to a Teknic motor (i.e. Hudson brushless servomotor), running the ST FOC SDK with speed control, we see that there seems to be some "charge-discharge" low-frequency sq...

0693W00000NrKMFQA3.png
c1ron by Associate III
  • 998 Views
  • 0 replies
  • 0 kudos

X-NUCLEO-IHM07M1 Motor Driver Board

The Quick Start Guide for this board implies it is compatible only with the following Nucleo boards:NUCLEO-F030R8NUCLEO-F103RBNUCLEO-F302R8NUCLEO-F401REDoes anyone know if it will work with any of the Nucleo F7 or H7 boards?

jerry2 by Senior
  • 1621 Views
  • 1 replies
  • 0 kudos

Where can i get the firmware of steval-spin3204??

Where can i get the firmware of steval-spin3204?? that is, stsw-spin3204.zip.I have the steval-spin3204 board for testing a motor.I try to automatically generate the firmware with X-CUBE-MCSDK-Y tool.Unfornately, I got the error of "freemarker templa...

AShin.5 by Associate II
  • 1726 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.