2022-05-27 12:51 PM
The Quick Start Guide for this board implies it is compatible only with the following Nucleo boards:
NUCLEO-F030R8
NUCLEO-F103RB
NUCLEO-F302R8
NUCLEO-F401RE
Does anyone know if it will work with any of the Nucleo F7 or H7 boards?
2022-05-29 11:17 AM
Hello @jerry2 ,
The X-NUCLEO-IHM07M1 is compatible with STM32 Nucleo boards, with the ST Morpho connector and supports the addition of other boards which can be stacked with onto a single STM32 Nucleo board.
Firstly, you should check if your board is pin to pin compatible with the headers, check the GPIO to enable the motor controller board.
You can adapt the available example (Eg: for NUCLEO-F401RE) to your board.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.