2022-10-18 5:49 AM
The MC Workbench tool generate a CubeMX 6.5.0 project, that in turns generate C code.
Actual behavior
When I select in this CubeMX project Project Manager > Code Generator > Copy only the necessary files, the generated IAR 8.0 project does not compile because a bunch of missing .h files (mainlay related to Low-Level lib, as the _ll_ in the name suggests).
Expected behavior
The generated IAR project should compile and there should not be missing files.
By the way, I note that LL functions are used despite in the MC Workbench I seleted "Use HAL" instead of LL.
This generates ~160 files instead of the ~1400 files, what is much easier to archive better environmental-friendly (less disk resource and network traffic).
Solved! Go to Solution.
2022-10-20 5:32 AM
Hello,
You are fully right.
For the moment, Motor Control part uses the LL whatever HAL/LL choice.
It is the reason why "Copy only the necessary files" will generate missing files errors.
Then, please, with current version, generate code with MC Work Bench or "Copy all used libraries" option on CubeMx".
Best regards.
GMA
2022-10-20 5:32 AM
Hello,
You are fully right.
For the moment, Motor Control part uses the LL whatever HAL/LL choice.
It is the reason why "Copy only the necessary files" will generate missing files errors.
Then, please, with current version, generate code with MC Work Bench or "Copy all used libraries" option on CubeMx".
Best regards.
GMA
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.