STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

UML Map of MC SDK?

The MC SDK is sometimes hard to follow. Has anyone made any UML maps of the SDK or know of any tools to generate these maps? I knew I saw a tool to do this long ago, but now I can't find it again. Seems like a tool that would be widely used. Than...

About FOC generated code with MCSDK

I am a newer leraning motor FOC control. I study the generated code by MCSDK tool with hall (120 degree). Below is some question:In file mc_config.c, about hall configuration ".hMaxReliableMecSpeedUnit     = (uint16_t)(1.15*MAX_APPLICATION_SPEED_UNI...

LLion.1 by Associate
  • 772 Views
  • 0 replies
  • 0 kudos

Connection Failed SPIN3204

Hi,I have a STEVAL-SPIN3204 board. I have opened the 6step_steval_spin3204 project on the ST motor control workbench, generated the code withe the following parameters using UPDATE button:STM32CubeMx: 6.5.0Target Toolchain: Keil MDK-ARM V5Firmware Pa...

dbuso.11 by Associate II
  • 649 Views
  • 0 replies
  • 0 kudos

Why cannot I get desirable PWM output?

Hi there,I'am using STEVAL-SPIN3201 evaluation board. I've reset PA11 for overcurrent output signal visible only to MCU and set PF6 and PF7 for overcurrent protection limit. Also, I've configured TIM1 channel 1 PA8 pin to center aligned pwm mode. Whe...

finding the cause for MOSFET burning STM32G431

Hey @ allthe setup: custom motor control PCBmicrocontroller: STM32G431CBU6gate-driver: UCC2721, 15Vthree shunt lowside current sense 150 µOhmOPAMP MAXIM MAX40056 20V/Vinverter stage: 24x IRF7759 (4 parallel)gate resistor 4,7 Ohmgate-source resistor 2...

0693W00000WHyo3QAD.png 0693W00000WHyuaQAD.png 0693W00000WHyv4QAD.png
ALedi.1 by Associate III
  • 1560 Views
  • 0 replies
  • 0 kudos

How to change polling of the Motor Pilot plot ?

Hello,In the documentation STM32 MC Motor Pilot :« Viewing and plotting registers with low-speed plotting.With this method of plot, any register can be plot but at low rate (polling every 200 ms by default) »I want to use the Motor Pilot plot (low sp...

Agran.1 by Associate II
  • 1371 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.