STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Motor not spinning

Hey guys,:eyes: I'm trying to drive a 3kw brushless motor using HALL sensors with a single shunt custom board, based on the stm32f103rb(LQFP64) with the following configuration:MCSDK_v5.4.7-FULLMCU: STM32F101RB, 72MHz, Ext ClockMotor parameters:24 po...

0693W00000Y8FvTQAV.png 0693W00000Y8IUVQA3.png
MOhir.1 by Associate
  • 1802 Views
  • 1 replies
  • 0 kudos

Erasing memory corresponding to segment 0: Erasing internal memory sectors [0 29] Error: failed to erase memory

Error: failed to erase memoryEncountered Error when opening C:\ST\STM32CubeIDE_1.11.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.500.202209151145\tools\bin\STM32_Programmer_CLI.exeError in STM32CubeProgrammer...

0693W00000Y8I1EQAV.png

I need to develop a controller for 2 Wheeler BLDC PMSM Hub Motor - 350W, 48V, with Hall sensor feedback.. Please suggest ST existing solutions - Development board + Firmware using which I can test performance on my 2 wheeler.

Plan is to use existing development boards from ST and test on 2 wheeler. Once performace is validated, we will modify the hardware and also develop additional peripheral firmware.Looking for both 6 STEP solution and also FOC.Regards,Anil

MC Workbench 6.1.0 CubemX 6.6.1 Code generation error when not "Copy all used libraries into the project folder" selected

I am using the latest motor control workbench (6.1.0) and the CubeMx (6.6.1). The motor control code generation is working if all the files copied to the project folder. If I select the "Copy only the necessary library files" some header files will m...

0693W00000Y8B5nQAF.png 0693W00000Y8B38QAF.png
lantiati by Associate II
  • 1689 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.