2023-01-12 11:03 PM
I am trying to evaluate STSPIN32F0251S1 ,
My requirement is use 6 steps ( trapezoidal ) implementation ,
I tried to use example project from motor control workbench 5.Y.4
[EVSPIN32F0251S1] + [Shinano LA052-080E3NL1] HW setup using
* the Six-Step algorithm Voltage modes and Sensorless
software packages
when i tried update motor parameter and Generate code is show some error (image attached) .
if choose the only update option then code generates but motor parameter remain same.
Need some help
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.