STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

How to control sensored motor via B-G431B-ESC1 PWM input ?

Hi all!I am trying to control a motor with integrated hall sensors using the B-G431B-ESC1. I've had a lot of problems, getting all kinds of errors while setting up the firmware, but I managed to control it through the motor pilot.Now I would like to ...

timco by Associate II
  • 4917 Views
  • 7 replies
  • 0 kudos

TImer 1 Break interrupt , false trigger

Hello Everyone,I trying to develop customize BLDC motor control code on STEVAL-STPIN3204 Timer 1 - Ch 1 to Ch 3 - PWM signal drive Ch 4 - No PWM output ModeI am providing the some pulse to Gate drivers please refer the image 1. After p...

MMand.3 by Associate
  • 1509 Views
  • 0 replies
  • 0 kudos

Driving BLDC 2000 Watt using STEVAL-CTM009

Hi,Currently I am working on two wheeler project with QS motor 2kW, for development purpose I use STEVAL-CTM009 and Nucleo-F103RB. I use lab bench supply (30V,3A) as VBUS.I tried to driving the BLDC with sensorless algorithm but after few seconds the...

ldanu by Associate II
  • 816 Views
  • 0 replies
  • 0 kudos

We’re building a motor controller and would like the Altium project files for the EVSPIN32F06Q1S3 evaluation board.

The motors (being controlled) will eventually be used in a man-rated system. We know this EVSPIN32F06Q1S3 reference design is for unmanned systems like drones, but we plan to start here. Do you know of a chip and reference design that is better suite...

JBrin.3 by Associate
  • 807 Views
  • 0 replies
  • 0 kudos

ADC Interrupt Generation difference

I am bit confused with ADC interrupt code generated for my project compared with the code generated from the motor control SDK for the evaluation board B-G431-ESC1.For my generated code void ADC1_2_IRQHandler(void){ /* USER CODE BEGIN ADC1_2_IRQn 0 *...

SRedd.5 by Senior III
  • 1025 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.