2023-03-15 4:10 AM
Hello Everyone,
I trying to develop customize BLDC motor control code on STEVAL-STPIN3204
Timer 1 - Ch 1 to Ch 3 - PWM signal drive
Ch 4 - No PWM output Mode
I am providing the some pulse to Gate drivers please refer the image 1.
After providing the pulse , and comparator 4 trigger then applied motor break , during motor break function , Timer 1 Break Interrupt Generated.
Break Function ()
{
TIM1->SR = ~(TIM_SR_UIF); // Clear the update Flag
TIM1->CCR1 = (uint32_t)0; // Clear the Pulse width 1
TIM1->CCR2 = (uint32_t)0; // Clear the Pulse width 2
TIM1->CCR3 = (uint32_t)0; // Clear the Pulse width 3
TIM1->CCR4 = (uint32_t)0; // Clear the Pulse width 4
TIM1->BDTR &= ~(TIM_BDTR_MOE); // Disable all output
TIM1->CCER &=(0xF555); // Reset the Channel Polarity
TIM1->EGR |= TIM_EGR_COMG; // Generate the event for execute the reset polarity (must required)
TIM1->BDTR |= TIM_BDTR_MOE; // Enable all output
}
IPD_pulse _Function()
{
((TIM1->CR1) &= ~((0x1UL << (0U))));
TIM1->CNT = 0;
TIM1->CCR1 = (uint32_t)0;
TIM1->CCR2 = (uint32_t)0;
TIM1->CCR3 = (uint32_t)0;
TIM1->CCR4 = (uint32_t)4150;
TIM1->BDTR &= ~(TIM_BDTR_MOE); // Disable all output
TIM1 -> CR1 &= ~TIM_CR1_UDIS;
TIM1->CCER &=(0xF555); // Reset the Channel Polarity
TIM1->EGR |= TIM_EGR_COMG; // Generate the event for execute the reset polarity (must required)
TIM1 -> CR1 |= TIM_CR1_UDIS;
(TIM1->CCER) |= ( LL_TIM_CHANNEL_CH1 | LL_TIM_CHANNEL_CH1N | LL_TIM_CHANNEL_CH2 | LL_TIM_CHANNEL_CH2N|LL_TIM_CHANNEL_CH3 | LL_TIM_CHANNEL_CH3N);
switch (commState)
{
case 1:
(TIM1->CCER) &= ~( LL_TIM_CHANNEL_CH1 |LL_TIM_CHANNEL_CH3 );
TIM1->CCER |= (LL_TIM_CHANNEL_CH2 | LL_TIM_CHANNEL_CH2N | LL_TIM_CHANNEL_CH1N | LL_TIM_CHANNEL_CH3N);
TIM1->CCR1 = (uint32_t)0;
TIM1->CCR2 = (uint32_t) IPD_PULSE;
TIM1->CCR3 = (uint32_t)0;
break;
case 2:
(TIM1->CCER) &= ~(LL_TIM_CHANNEL_CH2 );
TIM1->CCER |= (LL_TIM_CHANNEL_CH1 | LL_TIM_CHANNEL_CH3 | LL_TIM_CHANNEL_CH3N | LL_TIM_CHANNEL_CH2N | LL_TIM_CHANNEL_CH1N );
TIM1->CCR1 = (uint32_t)IPD_PULSE;
TIM1->CCR2 = (uint32_t)0;
TIM1->CCR3 = (uint32_t)IPD_PULSE;
break;
case 3:
(TIM1->CCER) &= ~( LL_TIM_CHANNEL_CH2 | LL_TIM_CHANNEL_CH1 );
TIM1->CCER |= ( LL_TIM_CHANNEL_CH2N | LL_TIM_CHANNEL_CH1N | LL_TIM_CHANNEL_CH3N | LL_TIM_CHANNEL_CH3);
TIM1->CCR1 = (uint32_t)0;
TIM1->CCR2 = (uint32_t)0;
TIM1->CCR3 = (uint32_t) IPD_PULSE ;
break;
case 4:
(TIM1->CCER) &= ~( LL_TIM_CHANNEL_CH3 );
TIM1->CCER |= (LL_TIM_CHANNEL_CH1 | LL_TIM_CHANNEL_CH2N | LL_TIM_CHANNEL_CH2 | LL_TIM_CHANNEL_CH1N | LL_TIM_CHANNEL_CH3N);
TIM1->CCR1 = (uint32_t)IPD_PULSE;
TIM1->CCR2 = (uint32_t)IPD_PULSE;
TIM1->CCR3 = (uint32_t)0;
break;
case 5:
(TIM1->CCER) &= ~( LL_TIM_CHANNEL_CH2 | LL_TIM_CHANNEL_CH3 );
TIM1->CCR1 = (uint32_t)IPD_PULSE;
TIM1->CCR2 = (uint32_t)0;
TIM1->CCR3 = (uint32_t)0;
TIM1->CCER |= (LL_TIM_CHANNEL_CH1 | LL_TIM_CHANNEL_CH2N | LL_TIM_CHANNEL_CH1N | LL_TIM_CHANNEL_CH3N);
break;
case 6:
(TIM1->CCER) &= ~( LL_TIM_CHANNEL_CH1);
TIM1->CCER |= (LL_TIM_CHANNEL_CH3 | LL_TIM_CHANNEL_CH2N | LL_TIM_CHANNEL_CH2 | LL_TIM_CHANNEL_CH1N | LL_TIM_CHANNEL_CH3N);
TIM1->CCR1 = (uint32_t)0;
TIM1->CCR2 = (uint32_t)IPD_PULSE;
TIM1->CCR3 = (uint32_t)IPD_PULSE;
break;
default:
break;
}
TIM1->EGR |= TIM_EGR_COMG; // Generate the event for execute the reset polarity (must required)
(TIM1->CR1) |= ((0x1UL << (0U)));
//TIM1->ARR = 0; // Set Auto Reload
TIM1->CNT = 0;
TIM1->RCR = 1;
TIM1 -> ARR = IPD_PULSE;
TIM1 -> CR1 &= ~TIM_CR1_UDIS;
TIM1 -> EGR = TIM_EGR_UG;
TIM1 -> CR1 |= TIM_CR1_UDIS;
TIM1->BDTR |= TIM_BDTR_MOE; // Enable all output
LL_TIM_SetTriggerOutput(TIM1, LL_TIM_TRGO_OC4REF); //Set the trigger output (TRGO) used for timer synchronization
TIM1->CCR4 = 3150; // Set the ADC R
TIM1->DIER |= TIM_DIER_CC4IE; // Enable interrupt on channel 4
LL_TIM_SetAutoReload(TIM1,4800); // set auto reload
}
Even i tried to remove the R44 resistor and C21 short to GND ,still at certain current level
Timer Break interrupt is Generated (please refer the schematic)
Please anyone can guide me for same?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.