2023-03-12 9:55 AM
I am bit confused with ADC interrupt code generated for my project compared with the code generated from the motor control SDK for the evaluation board B-G431-ESC1.
For my generated code
void ADC1_2_IRQHandler(void)
{
/* USER CODE BEGIN ADC1_2_IRQn 0 */
/* USER CODE END ADC1_2_IRQn 0 */
HAL_ADC_IRQHandler(&hadc1);
HAL_ADC_IRQHandler(&hadc2);
/* USER CODE BEGIN ADC1_2_IRQn 1 */
/* USER CODE END ADC1_2_IRQn 1 */
}
The
HAL_ADC_IRQHandler(&hadc1);
HAL_ADC_IRQHandler(&hadc2);
are generated,
but for the motor control SDK i find it
void ADC1_2_IRQHandler(void)
{
/* USER CODE BEGIN ADC1_2_IRQn 0 */
/* USER CODE END ADC1_2_IRQn 0 */
// Clear Flags M1
LL_ADC_ClearFlag_JEOS( ADC1 );
(void)TSK_HighFrequencyTask();
/* USER CODE BEGIN HighFreq */
/* USER CODE END HighFreq */
/* USER CODE BEGIN ADC1_2_IRQn 1 */
/* USER CODE END ADC1_2_IRQn 1 */
}
I understand the (void)TSK_HighFrequencyTask(); is a user code but how
// Clear Flags M1
LL_ADC_ClearFlag_JEOS( ADC1 ); is generated? Is there any selection? Please help.
.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.