STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

Resolved! using stm32wl55ccu to drive 3 phase bldc

Hi ,I am using stm32wl55ccu 48 pin QFN MCU to drive a 3 phase brushless motor using 3-phase complementary PWM output signals using TIMER 1. I have seen at the datasheet that this 48 QFN package is missing the complementary output of TIMER1 ,Channel 3...

YY55 by Associate
  • 1836 Views
  • 1 replies
  • 1 kudos

Get motor to run at board power-up.

Is there a parameter where I can set the motor speed so that when the board is powered on the motor starts at a given rpm?I am fairly new to this but have managed to get a motor profile and generated a code but my knowledge stops there.board: B-G431B...

MEika.1 by Associate
  • 1390 Views
  • 1 replies
  • 0 kudos

MCSDK / FOC SDK for STM32F2

Hello, I have read that the support for STM32F2 in FOC SDK / MCSDK is skipped after 4.x. Is that right, if so, where can I get the latest 4.x version for my STM32F2 design? Thanks in advanced

MiJes by Associate II
  • 1503 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.