STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9745 Views
  • 5 replies
  • 3 kudos

3 phase PWM Commutation

Hello,I am using Timer 1 for the generation of 3PWM and their complimentary Signals and I am getting all 6 PWM waveforms.For six step commutation I need to add phase delay between the channels of the timer. Is it possible using any HAL function? I am...

ajishsaji by Associate II
  • 11780 Views
  • 12 replies
  • 1 kudos

Resolved! MCSDK motor startup short circuit

Hello, when referencing a position control with a new custom hardware, there is a short circuit of the power supply at the beginning of the referencing. The STM32 G4 with the MCSDK 5.4.8 is used. The setup already ran on a first own board so that the...

julian3 by Associate
  • 1896 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H7 hardfault from random point in code

Hi all.I develop controller for PMSM motor and got a problem as below:Some time MCU jump to hardfault handler. In debug, I see that it cause from random point (different from time to time), some time it cause from very basic function (such as sinf(),...

dinhlx_0-1693564942608.png dinhlx_0-1693566061460.png dinhlx_0-1693579899408.png dinhlx_1-1693579988094.png
dinhlx by Associate II
  • 5389 Views
  • 6 replies
  • 2 kudos

startup of steval-spin3204

hello STM technical Team,I Subodh Sawant, working with Senergy intellution, India.Now we are working with BLDC motor with FOC algorithm and we purchased STEVAL-SPIN3204.We installed all required software.Problems facing:1) we are not able to establis...

Subodh_Sawant_39_0-1694261747672.png Subodh_Sawant_39_1-1694261839956.png

MCSDK 6 board config

Using the SDK I am basing a new system on the EVSPIN32G4. After selecting the inverter, and motor, I am then taken into the parameter configuration of the motor driver.According to the boards manager the EVSPIN32G4 has multiple configurations availab...

Motor control fails after motor stop

I am using an e-bike motor 48V350W with an EVALSTDRIVE101 3Sh and NUCleo F401REboard to do some tests. The motor only starts the first time I press start and then if I stop it doesn't resume rotation unless I restart the Nucleo board. I analyzed the...

MLasc.1 by Associate
  • 1445 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.