STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

Resolved! STM32 Motor Control - STM32G474xx - HRTIM Support?

Hello,Are there any future plans to add HRTIM Support in ST Motor Contol Workbench? As far as i have seen G474 is inculded, but only with TIM1 and TIM8. Though these two are the advanced motor control timers, i need a faster PWM signal for my applica...

GPoll.1 by Associate
  • 2797 Views
  • 2 replies
  • 0 kudos

B-G431B-ESC1 is bidirectional?

I intend to drive a BLDC with regenerative braking. i would like to know if the B-G431B-ESC1 component works bidirectionality, since during the regenerative braking there will be current return. I will also integrade a Buck/Boost DC-DC bidirectional ...

B-G431B-ESC1 with MCSDK6.0: API documentation

Hello, I am new to the ST motor control workbench.Already did the the initial steps of reading UM3027 and using the profiler and MC-SDK v6.0 Workbench GUI to generate a CubeIDE project.The generated project only does initialization. The while loop is...

DGuim.1 by Associate
  • 2110 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.