STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Resolved! trouble with B-G431-ESC1

Hi, I have been working with the B-G431-ESC1 for some time.I profiled my motor with ST Profiler and loaded the .JSON file on Workbench and generated the code.My final goal is to be able to control the speed of my motor by sending a PWM signal to the ...

Jess32 by Associate II
  • 2612 Views
  • 2 replies
  • 0 kudos

Board Manager custom board: pin selection

We're implementing our own inverter board based on a G431 controller. I'm currently going through all the required parts and I'm wondering how I am supposed to know the pins I can use for certain features.Example: motorDrives, feature: CurrentSensing...

DMeie.2 by Senior II
  • 1632 Views
  • 2 replies
  • 1 kudos

Resolved! Block Diagram of FOC

Hi Team,If anyone has, could you please share the application note for the Motor control Applications for NUCLEO-G431RB and X-NUCLEO-IHM16M1.If anyone has the block diagram of the FOC also, Please share 

About board EVSPIN32G4

Hello, I need help the product I mentioned EVSPIN32G4 I've been trying for a long time to find the pins on the board to control GPIO signals instead of SPI InterfaceI need to find these pins on the board:I/O control terminalGND Ground wireF/R Forward...

How to controll esc with pwm signal from RC controller

So i have this simple code for pwm input for the rc controller :void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef* htim){if (htim->Instance == TIM2){if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1){capture_value[0] = HAL_TIM_ReadCapturedValue(htim, TIM...

Matyáš by Associate II
  • 7283 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.