2022-07-15 8:05 AM
i want to create a firmware for the stspin32g4 mcu but the cubeMx let me not select this mcu. in fact no spin mcu. i can not select a mcu with name spin
cubemx bug or st now not support the mcu with integrated drivers?
2022-07-15 8:09 AM
i have cubeMx 6.5.0 on windows 10
in the IDE is the same, i can not select a spinXXX mcu
2022-07-16 4:58 AM
As the stspin32g4 includes a STM32G431VB, you should be able to work by selecting that one.
2024-02-26 1:24 AM
I encountered the same problem, it can be used, but for HW egineer it is lacking the function of knowing your possibilites where to pin swap alternate functions etc. because you have not got the reference to avalailable pins on STSPIN32 package, you have to do a lot of workarounding to at least get an idea.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.