STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4994 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9747 Views
  • 5 replies
  • 3 kudos

How to upload STEVAL-ESC002V1?

I bought a STEVAL-ESC002V1 board and I don't know how to customize its firmware. I downloaded STM32CUDE IDE and Motor Control Workbench but none of than have a board option for STEVAL-ESC002V1 nor STSPIN32F0A. So, I downloaded the STSW-ESC002V1 which...

ACho.11 by Associate II
  • 1757 Views
  • 1 replies
  • 0 kudos

Regarding motor low RPM not achieved

I have a BLDC motor equipped with Hall sensors. When attempting to run the motor in FOC (Field-Oriented Control) mode, I encountered difficulties achieving the required low RPM. Consequently, I configured the Hall sensors to run the motor, but encoun...

suhas1 by Associate II
  • 1491 Views
  • 1 replies
  • 0 kudos

Evspin32G4-dual : Turning 2 motors simultaneously

Hello,I have an EVSPIN32G4-Dual, I am Trying to Run 2 HooverBoard Motors (36V/15A/510RPM/HALL).I generated the firmware using Mc Workbench 6.2.1 and desabled the overcurrent protection for stage 2. Then tried to command the motors using motor pilot, ...

ItzSam by Associate II
  • 1816 Views
  • 2 replies
  • 0 kudos

Motor is not spinning

Dear all,I have a NUCLEO-F302R8 and the X-NUCLEO-IHM07M1 motor driver expansion board. I have a three phase BLDC motor with an encoder attached to it. I have profiled the motor and I am able to run the motor in the profiler. When I use the workbench ...

nonameX by Associate
  • 1510 Views
  • 1 replies
  • 0 kudos

ACIM example change MCU to 48 pin

Dear support,I am designing a ACIM driver. I want to change MCU to 48 pin LQFP package. but example is only has 64pin MCUHow can I change to MCU type?thanks for your helps

Mnemonic by Associate III
  • 914 Views
  • 0 replies
  • 0 kudos

Resolved! STSPIN32G4. sensorless tuning

Hello,For our battery-powered smoke extraction fans, we want to develop a brushless motor driver 1.5KW.For this new development we use the reference STSPIN32G4.I use a custom EVSPIN32G4 circuit board with a 4 pole pairs brushless motor equipped with ...

JLC by Associate II
  • 3245 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.