STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

error in MX generating from MC workbench

Hello, Please I need a help, I'm using the MC workbench and after saving the project and reach to generate the project it's giving this error that the MX is not found or I need to install a verison more the 6.0. bytheway I already installed the lates...

Dandan by Associate
  • 1538 Views
  • 1 replies
  • 0 kudos

Clark and Park implementation code

This is the first time I have to implement a PMDC motor control system.There are 3-phase sine currents need to be converted into d-q components using Clark and Park.I don't have the motor to test yet, so with the DAC I created three 120° phase-shifte...

luke514_0-1710682162081.png
luke514 by Senior
  • 3636 Views
  • 1 replies
  • 0 kudos

STSPIN32G4 LPUART for MCP?

[VERSION]: 6.2.1[TOOL]: MC WB, Board Manager[DETAILS]: I'm working with a custom board using an STSPIN32G4. Can the LPUART on the STSPIN32G4 be used for the MCP (Motion Control Protocol)? When I try assigning the pins for the LPUART (PB10 and PC1) to...

AaronP_1-1710179599112.png AaronP_2-1710179709699.png
AaronP by Associate
  • 1364 Views
  • 1 replies
  • 0 kudos

Schematic for stspin32 and mosfet recommendation

Hi GuysI'm just a newbie who got into stm32 architecture and i want to develop a BLDC controller for a Flycat 5010 360kv BLDC motor the power supply is 24v and the max current rating i want is 60A can anyone recommend me a schematic a application not...

X-Nucleo-IHM03A1

Good morningI am in the process of building another CNC milling machine. For the two largest stepper motors , I would like to use X-Nucleo-IHM03A1 drivers connected to the Stm32 board. I initially looked at the capabilities of IHM03A1 and batch files...

Janusz53 by Associate
  • 1069 Views
  • 1 replies
  • 0 kudos

MC SDK 6.2.1 doesn't launch after installation

Hello, I do have a problem running STM32 Motor Control Workbench 6.2.1 . The UI doesn't load at all. even running with admin rights and installed using admin rights as well   I have downloaded Microsoft Visual C++ Redistributable Version 14.38.33135....

aabdelghany_0-1710495762079.png

Break interrupt keeps firing

Hi allI have some problem using the Break interrupts (BK1 and BK2). When activated it keeps firing the break interrupt handler: TIM1_BRK_IRQHandlerWe have measured the BK1 and BK2 signals and the states are as they scould be when activayted/deactivat...

TJO_0-1710420693830.png
TJO by Associate
  • 2174 Views
  • 3 replies
  • 0 kudos

controlling servo motors in high frequency with stm32

Hello all,I'm trying to learn how to control multiple servo motors with STM32.I need to run my servos at 333Hz - and I don't know how to change the frequency from the default frequency?Could anyone help me please - any example code / guide will be mu...

galporat by Associate
  • 2697 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.