2024-03-14 9:59 AM
Hi Guys
I'm just a newbie who got into stm32 architecture and i want to develop a BLDC controller for a Flycat 5010 360kv BLDC motor the power supply is 24v and the max current rating i want is 60A can anyone recommend me a schematic a application note to hook up the MCU and Recommend a mosfet to handle the above mentioned spec any help would be appreciated.
Thank you
Kavin kumar
2024-03-15 2:36 AM
Hello kavinkumar,
Currently the MCSDK supports very few boards that can sustain such current levels, and seeing the kind of motor you want to use, I can't help to wonder if that is really necessary. Would you be so kind as to elaborate on the type of application you want to go into ? Is the board only meant for motor control ? Are you planning on running several of these motors on the same board ?
2024-03-15 4:09 AM
I want to make FOC Bldc controller board for a Quadruped robot where each motor has a separate Mcu and only one motor will be driven under one MCU
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.