2024-03-18 2:49 AM
Hello Everyone,
I would like to use STM32F373xx series. However I noticed in the datasheet, they don't specify PWM generation with "edge or center-aligned modes" with full modulation capability (0-100%)?
Is this MCU can generate PWM with center-aligned mode and can I use It for motor control application ?
Need your help!
Regards,
2024-03-18 3:19 AM
> I noticed in the datasheet, they don't specify PWM generation with "edge or center-aligned modes" with full modulation capability (0-100%)?
This formulation for other STM32 is in the Advanced Timer chapter of DS. STM32F373 is a rare exception which does not have any Advanced Timer (in all STM32 they are consistently numbered as TIM1, TIM8 and TIM20). These timers feature 3 channels with complementary outputs with dead-time insertion and BREAK capability. STM32F373 does have TIM15-TIM17 which have complementary outputs and BREAK capability, but they are simpler than the Advanced timers and have only 1 or 2 channels instead of 3.
However, if you don't need any of the listed features, all timers which do have outputs, can output 0-100% PWM.
> can I use It for motor control application ?
That's a vague question, the answer depends on what motor exactly do you want to control and exactrly how.
You may want to look at other STM32, too; perhaps the 'G4 family, which is a newer successor to the 'F3 family.
JW
2024-03-18 6:23 AM
Thank for your quick reply.
Indeed, I would like to design a DC motor in the application requirement : PWM generation (edge or center-aligned modes) needed to attenuate current noise measurement. Can the STM32F373xx do this or should I go for 'G4 family?
2024-03-18 7:05 AM
Sorry, I don't know, I don't design DC motor control applications, I've just described you the capabilities of the chip in general.
JW
2024-03-18 7:12 AM
Alright, thank you for your help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.