STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1837 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4991 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

Resolved! OCP in custom board

I have over current protection like this in my custom board how can i implement this on motor control workbench here is my file and i'm getting eror when i try create with six step 

Screenshot 2024-04-07 220844.png Screenshot 2024-04-07 220859.png
TKara.2 by Associate III
  • 3234 Views
  • 6 replies
  • 0 kudos

Resolved! PWM behavior when changing deadtime during operation

Hello!I'm having some issue while updating the deadtime of the PWMs on Advance timer TIM1 during PWM operation is running.I'm attaching the scopeshot with the Channel 1 and 1N pulses, during deadtime register(DTGbin) update ,the deadtime is zero. In ...

photo_pwm_deadtime_1.jpg photo_pwm_deadtime_2.jpg

I can't complete ST Motor Profiling

Hello, Hardware : NUCLEO-G474RE + X-NUCLEO-IHM08M1 + DollaTek 2204 BLDC motorSoftware : Motor Control Benchwork 6.2.1, STM32CubeIDE 1.13.1 When I try to start motor profiling the motor starts to produce radom beeps, vibrations and accidental spins. T...

mikde by Associate
  • 3889 Views
  • 3 replies
  • 0 kudos

Position Control with Quadrature Encoders

Hi,I am trying to create a User Application where I pass in commands from a terminal application (ex: Putty or Ucon) which results in the motor doing something.I have configured the MC Workbench with the following options:   Not using the MC Pilot so...

smaiti_0-1704304765448.png smaiti_1-1704304797449.png smaiti_3-1704304919032.png
smaiti by Associate III
  • 7114 Views
  • 8 replies
  • 0 kudos

Motor Power Calculation (Watt)

Hello, I am working on a motor control project that is to be driven battery-powered. This means that the DC current has to be monitored in order to avoid overloading the battery. I have made a Control Loop which takes in a DC Current reference as inp...

MC_STEVAL_FOC_5A_Current_Limit_v3.png {6248B94D-DE7D-40BE-9ED5-2D173B42E8C9}.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.