STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9744 Views
  • 5 replies
  • 3 kudos

Resolved! Motor setting for B-G431B-ESC1

Hello eveybody.Before try to uss a motor with encoder drive by B-G431B-ESC1 board, need some setting ? Examples:Encoder A and B sequence respect to motor rotation CW or CCW ?Encoder phased to electrical motor phase ?Any Other ?

UniRob by Associate III
  • 3291 Views
  • 4 replies
  • 0 kudos

Resolved! FOC control of 2 motors

I am currently working with a STM32G431RB and X-Nucleo-IHM08M1 and a motor with Halls. I want to drive 2 motors independently with the control board. Workbench seems to allow for 2 motors with FOC but not with the STM32G431RB.In fact, there appears t...

Motorcontrol

I want to display the current updates, speed, and voltage of the motor on an ST7735 display. I'm facing a problem where the variables are not updating the values. Could you help me as soon as possible?"

karthic by Associate
  • 891 Views
  • 0 replies
  • 0 kudos

motorbench 6.2.1 with cube MX

Hello,I have intsalled the motorbench version 6.2.1, and I have already the cubeMX version 6.9, but when I'm using the motorbench and trying to open an example for the steval-spin3201, it's working until I reach the generate program and it's saying a...

Dandan0707_0-1713341768523.png

Resolved! High power BLDC controller

Hello Team,  We want to develop a BDLC driver with high power. We went through the below product, it matches other requirements except for output current, it is only up to 1.5AMotor Control Nucleo Pack with NUCLEO-G431RB and X-NUCLEO-IHM16M1can u sug...

sshin.9 by Associate II
  • 1143 Views
  • 1 replies
  • 0 kudos

Rev-Up phases and meaning

What is the meaning of the five different rev-up (start-up) phases that one can set up in sensorless mode?From my experiments, I figured that Phase 1 is alignment and Phase 2 is an actual startup phase. Is this correct? What are the other phases for?...

DMeie.2 by Senior II
  • 2895 Views
  • 3 replies
  • 3 kudos

BEMF goes the wrong way

HiI am struggling with the appearance of my BEMF in my 6 step control.The picture shows one of the phases. And according to all the documentation I've seen ( and I have read a lot ) my BEMF goes the wrong way. The BEMF looks like outstanding ears but...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.