STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1839 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Compatibility of STM32U Series with MCSDK

Hi,I'm working on a motor control project using STM32 microcontrollers and plan to use the Motor Control Software Development Kit (MCSDK).I noticed that the STM32U series isn't listed in the wiki for MCSDK compatibility, which currently includes the ...

wow by Associate II
  • 2826 Views
  • 4 replies
  • 0 kudos

Error when generating code with MC Workbench 6.3.0

Hello there,I am currently working on a project considering the B G431B ESC1 and a BLDC motor.My goal is to control the motor through a external PWM Signal from a nucleo board.So far I could only control the BLDC motor through the MC Profiler and onl...

STMBatu by Associate II
  • 5672 Views
  • 7 replies
  • 0 kudos

Resolved! Excessive current on startup - Rev-up setting is ignored

[Basic Info]We're currently having issues with our custom board.It is based on the G431RB in FOC and 3-Shunt mode, with a DRV8323RS as the gate drive and for amplifying and attenuating the current measurement.The motor is a low-inductance (8.1µH) hig...

DMeie.2 by Senior II
  • 2633 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.