STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1838 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4992 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9746 Views
  • 5 replies
  • 3 kudos

Resolved! How to invert current reading?

For our motor control project we're using a driver IC with integrated opamp stage intended for current measurement.This opamp stage inverts the current reading compared to the Current sensing signals conditioning model, see here:To correct the curren...

grafik.png
DMeie.2 by Senior II
  • 3653 Views
  • 6 replies
  • 2 kudos

MDSK5.4.8 CAN Communication Not working

hi.I using MDSK 5.4.8 with NUCLEO F103RB / NUCLEO IMH07M1The speed control operation was confirmed through the variable volume.So now, I want to operate CAN 2.0A CommunicationI already set CUBEMX pin & CAN setting.Now, i just send message(tx test) De...

chocho by Associate II
  • 2437 Views
  • 1 replies
  • 0 kudos

Motor speed issues B-G431B-ESC1

Hi!Trying to use a Leopard LC2830-980KV motor with the B-G431B-ESC1. I have managed to program the device with the MC Workbench and can run the motor using the Motor Pilot software. However I can't seem to get the speed over 2100 rpm for some reason....

Skärmklipp3.PNG Skärmklipp4.PNG Skärmklipp2.PNG

Resolved! PWM input problem with B-G431B-ESC1

HI, I am currently doing a project with the B-G431B-ESC1. I am trying to control a motor with the B-G431B-ESC1. I already have profil my motor with the motor profiler software. I am able to control my motor with the motor pilot software. Now, I am tr...

elag by Associate
  • 2980 Views
  • 4 replies
  • 2 kudos

Resolved! Motor Pilot RegDesc cannot input float data

I added a custom REG in Motor Pilot and edited the MC_FOC_SDK.qml file, which allows usage, but I can only input integers, not floating-point data. Here is the configuration information. RegListSTMV2.json {    "Id" : 162,    "Name" : "OVER_BUS_CURREN...

honkerhz_0-1716439248602.png
honkerhz by Associate II
  • 1336 Views
  • 1 replies
  • 1 kudos

Resolved! AC current sense sine wave

Hi everyoneWe are checking phase current sense  in sine wave .in trapezoidal wave ac current controlled method  when the time phase passing pulse to get values. Sine wave how to current sense in low side triple shunt method. If any one knowlet me kno...

EVSPIN32F06Q2S1 and Refrigerator: Problems

HelloI'm trying to run a refrigerator compressor (basically a PMSM) with EVSPIN32F06Q2S1. I downloaded all necessary programs and started the MC Workbench, configured the board in sensorless FOC and uploaded the code to it. All that works fine. But w...

L_e_o by Associate II
  • 5243 Views
  • 4 replies
  • 0 kudos

Resolved! Workbench_6.3.0 Motor Control Protocol Rx 0F 04 04 C0

Using the motor control program generated by Workbench_6.3.0, Motor Pilot_6 can communicate normally. However, when sending manually using a serial port assistant, it always replies with 0F 04 04 C0 and cannot communicate normally. This issue does no...

honkerhz by Associate II
  • 1742 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.